[S32K11x] Questions about the function difference between FTM0 and FTM1

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

[S32K11x] Questions about the function difference between FTM0 and FTM1

952件の閲覧回数
GavinLi1
Contributor III

Dear NXP experts,

As the table shows in the RM,  I've some questions:

GavinLi1_0-1728631128045.png

Q1. Only FTM0 can output PMW but FTM1 not?

Q2. If I want to do the motor control, only FTM0 can be used, but FTM1 not support that, right?

Q3. Only FTM1 support input capture, but FTM0 not, right?

Thanks!

Gavin

0 件の賞賛
返信
1 返信

910件の閲覧回数
_Leo_
NXP TechSupport
NXP TechSupport

Hi,

Thank you so much for your interest in our products and for using our community.

With all FTM modules you can perform all modes described in Table 47-5. Channel Modes Selection.

FTM modulation, Quadrature Decoder, Hall sensor support and Dithering are particular modes that are only available in some FTM modules, like is described in Table 47-1. FTM instances and features. For these modes you can refer to their respective section in FTM chapter of reference manual.

Hope it helps you.

Have a nice day!

0 件の賞賛
返信