[S32K11x] Questions about the function difference between FTM0 and FTM1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[S32K11x] Questions about the function difference between FTM0 and FTM1

953 Views
GavinLi1
Contributor III

Dear NXP experts,

As the table shows in the RM,  I've some questions:

GavinLi1_0-1728631128045.png

Q1. Only FTM0 can output PMW but FTM1 not?

Q2. If I want to do the motor control, only FTM0 can be used, but FTM1 not support that, right?

Q3. Only FTM1 support input capture, but FTM0 not, right?

Thanks!

Gavin

0 Kudos
Reply
1 Reply

911 Views
_Leo_
NXP TechSupport
NXP TechSupport

Hi,

Thank you so much for your interest in our products and for using our community.

With all FTM modules you can perform all modes described in Table 47-5. Channel Modes Selection.

FTM modulation, Quadrature Decoder, Hall sensor support and Dithering are particular modes that are only available in some FTM modules, like is described in Table 47-1. FTM instances and features. For these modes you can refer to their respective section in FTM chapter of reference manual.

Hope it helps you.

Have a nice day!

0 Kudos
Reply