S32K118 PIN

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,172件の閲覧回数
wenfengyao
Contributor II

We need to input the external high-low level signal to the 18 pin of the MCU in series with a diode. At the beginning, the pin is in the default state without configuration, and only the external interrupt is used. In this case, the MCU pin detected at low level has a voltage of 800 or 900mV; When this pin is configured to the input (floating) state, the detected MCU pin has a voltage of about 0V at low voltage.

Our software colleagues believe that the external interrupt input and the configuration pin input (floating) should be in a high resistance state, but the measured results are not the same, may I ask the specific difference between the two internal circuits? What causes the low level input to have a voltage difference?

The part number is FS32K118LAT0MLFT

0 件の賞賛
返信
1 解決策
3,165件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @wenfengyao,

It should be in HIGH-Z and the pin should read 0V in this case unless there is the internal pull-up enabled - which would explain the 900mV at the anode.

The pullup is enabled on PTC5 by default, for example.

Which pin do you use?

What is the usecase here?

 

Regards,

Daniel

 

 

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
3,166件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @wenfengyao,

It should be in HIGH-Z and the pin should read 0V in this case unless there is the internal pull-up enabled - which would explain the 900mV at the anode.

The pullup is enabled on PTC5 by default, for example.

Which pin do you use?

What is the usecase here?

 

Regards,

Daniel

 

 

0 件の賞賛
返信
3,123件の閲覧回数
wenfengyao
Contributor II
I just want to use PIN 18 PTC5 pin to do an interrupt input, so the default state of this pin is pull-up?
0 件の賞賛
返信
3,114件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @wenfengyao,

PTC5 has internal pullup enabled by default out of reset.

Please refer to

S32K118 IO_Signal_Description_Input_Multiplexing.xlsx

IO SIgnal Table

Column S

 

Regards,

Daniel

0 件の賞賛
返信