S32K1 Series chip develop &debugger tool chain

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K1 Series chip develop &debugger tool chain

ソリューションへジャンプ
2,421件の閲覧回数
PedroCao
Contributor I

#S32K1

We will use the S32K1 series chip and are currently preparing to purchase the developing &debugger tool chains. Which software and hardware are required, including IDEs, compilers, debuggers, and others?

Can you share a detailed list of the tool chains and  introduce what is free and what needs to be purchased?

In addition, we currently have UAD2pro, can it be used as a debugger?

 

TKS

0 件の賞賛
返信
1 解決策
2,411件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@PedroCao

1.The IDE and SDK of S32K1 are provided to users free of charge, the only thing you need to worry about is to purchase a suitable debugger. Commonly used debuggers are recommended: PE, J-LINK and Lauterbach.

2.There are not many customers using UAD2pro, but I think it supports S32K1. For details, you need to confirm with UAD2pro's technical support.

 

3.For IDE I recommend users to install two versions
1. S32 Design Studio for Arm 2018 or V2.2.

          Although these two versions are very old, many released demos are based on this version.

2.S32 Design Studio Platform V3.5,

         the latest platform, can install RTD driver for MCAL requirement.

元の投稿で解決策を見る

2 返答(返信)
2,412件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@PedroCao

1.The IDE and SDK of S32K1 are provided to users free of charge, the only thing you need to worry about is to purchase a suitable debugger. Commonly used debuggers are recommended: PE, J-LINK and Lauterbach.

2.There are not many customers using UAD2pro, but I think it supports S32K1. For details, you need to confirm with UAD2pro's technical support.

 

3.For IDE I recommend users to install two versions
1. S32 Design Studio for Arm 2018 or V2.2.

          Although these two versions are very old, many released demos are based on this version.

2.S32 Design Studio Platform V3.5,

         the latest platform, can install RTD driver for MCAL requirement.

2,370件の閲覧回数
PedroCao
Contributor I
Many tks
0 件の賞賛
返信