S32K1 Series chip develop &debugger tool chain

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K1 Series chip develop &debugger tool chain

Jump to solution
2,409 Views
PedroCao
Contributor I

#S32K1

We will use the S32K1 series chip and are currently preparing to purchase the developing &debugger tool chains. Which software and hardware are required, including IDEs, compilers, debuggers, and others?

Can you share a detailed list of the tool chains and  introduce what is free and what needs to be purchased?

In addition, we currently have UAD2pro, can it be used as a debugger?

 

TKS

0 Kudos
Reply
1 Solution
2,399 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@PedroCao

1.The IDE and SDK of S32K1 are provided to users free of charge, the only thing you need to worry about is to purchase a suitable debugger. Commonly used debuggers are recommended: PE, J-LINK and Lauterbach.

2.There are not many customers using UAD2pro, but I think it supports S32K1. For details, you need to confirm with UAD2pro's technical support.

 

3.For IDE I recommend users to install two versions
1. S32 Design Studio for Arm 2018 or V2.2.

          Although these two versions are very old, many released demos are based on this version.

2.S32 Design Studio Platform V3.5,

         the latest platform, can install RTD driver for MCAL requirement.

View solution in original post

2 Replies
2,400 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@PedroCao

1.The IDE and SDK of S32K1 are provided to users free of charge, the only thing you need to worry about is to purchase a suitable debugger. Commonly used debuggers are recommended: PE, J-LINK and Lauterbach.

2.There are not many customers using UAD2pro, but I think it supports S32K1. For details, you need to confirm with UAD2pro's technical support.

 

3.For IDE I recommend users to install two versions
1. S32 Design Studio for Arm 2018 or V2.2.

          Although these two versions are very old, many released demos are based on this version.

2.S32 Design Studio Platform V3.5,

         the latest platform, can install RTD driver for MCAL requirement.

2,358 Views
PedroCao
Contributor I
Many tks
0 Kudos
Reply