S32K-PMSM Sensorless FreeMASTER issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K-PMSM Sensorless FreeMASTER issue

Jump to solution
5,359 Views
bjrajendra
Senior Contributor I

Hello all,

I'm trying to use PMSM SW downloaded from the NXP website. Accordingly I want to use its FreeMaster tool. But When I'm trying open the corresponding FreeMaster control, Im getting the pop-up error stating incorrect file handle was associated with it.

Kindly help in solving this issue.

Thanks in advance,

BJ Rajendranath

0 Kudos
Reply
1 Solution
5,193 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi Raju,

Which FreeMaster version are you using?

If an old one, could you please download and use the up-to-date version 2.0.9?

FreeMASTER Run-Time Debugging Tool | NXP 

Thank you,

BR, Daniel

View solution in original post

0 Kudos
Reply
3 Replies
5,193 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello,

I'm not able to reproduce the error.

Did you follow all the steps described in the MTRDEVKSPNK144 Quick Start Guide or here: Getting Started with MTRDEVKSPNK144 | NXP 

Is the FreeMaster tool installed?

Thanks,

BR, Daniel

0 Kudos
Reply
5,191 Views
bjrajendra
Senior Contributor I

Hi Daniel,

Thanks for your response.

In fact I just opened the FreeMaster Application which was there in the project. I did shown like this.

I'm having a doubt that Do we need to Run the Project to Open this File ?

Thanks & Regards

Raju

0 Kudos
Reply
5,194 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi Raju,

Which FreeMaster version are you using?

If an old one, could you please download and use the up-to-date version 2.0.9?

FreeMASTER Run-Time Debugging Tool | NXP 

Thank you,

BR, Daniel

0 Kudos
Reply