Can not flash s32K144

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can not flash s32K144

1,455 Views
cuongtran
Contributor II

I tried to flash the s32K144 device using S32 DS and I got the above error.  Can you help me out on this?.

Thanks.

0 Kudos
Reply
3 Replies

1,363 Views
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Cuong Tran

You forgot to attach the image of the error code that you have.

Regards

Jorge Alcala

0 Kudos
Reply

1,363 Views
cuongtran
Contributor II

Here is the error.

Thanks.

Cuong Tran, P. Eng.

Senior Software Engineer

Mechatronics

CLOSURES TECHNICAL CENTRE

521 Newpark Blvd., P.O. Box 354 Stn. Main

Newmarket, Ontario L3Y 4X7 Canada

OFFICE: +1 905-898-6744 x2187

e-mail:cuong.tran@magna.com

0 Kudos
Reply

1,363 Views
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Cuong Tran

Did you create the launch configuration? or it is a project imported from other environment?

Please verify that you have the following configuration in your configuration:

pastedImage_1.png

Regards

Jorge Alcala

0 Kudos
Reply