S32K-PMSM Sensorless FreeMASTER issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K-PMSM Sensorless FreeMASTER issue

ソリューションへジャンプ
5,356件の閲覧回数
bjrajendra
Senior Contributor I

Hello all,

I'm trying to use PMSM SW downloaded from the NXP website. Accordingly I want to use its FreeMaster tool. But When I'm trying open the corresponding FreeMaster control, Im getting the pop-up error stating incorrect file handle was associated with it.

Kindly help in solving this issue.

Thanks in advance,

BJ Rajendranath

タグ(1)
0 件の賞賛
返信
1 解決策
5,190件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi Raju,

Which FreeMaster version are you using?

If an old one, could you please download and use the up-to-date version 2.0.9?

FreeMASTER Run-Time Debugging Tool | NXP 

Thank you,

BR, Daniel

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
5,190件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hello,

I'm not able to reproduce the error.

Did you follow all the steps described in the MTRDEVKSPNK144 Quick Start Guide or here: Getting Started with MTRDEVKSPNK144 | NXP 

Is the FreeMaster tool installed?

Thanks,

BR, Daniel

0 件の賞賛
返信
5,188件の閲覧回数
bjrajendra
Senior Contributor I

Hi Daniel,

Thanks for your response.

In fact I just opened the FreeMaster Application which was there in the project. I did shown like this.

I'm having a doubt that Do we need to Run the Project to Open this File ?

Thanks & Regards

Raju

0 件の賞賛
返信
5,191件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi Raju,

Which FreeMaster version are you using?

If an old one, could you please download and use the up-to-date version 2.0.9?

FreeMASTER Run-Time Debugging Tool | NXP 

Thank you,

BR, Daniel

0 件の賞賛
返信