S32DS Generator: ERROR

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32DS Generator: ERROR

1,933 次查看
Jackson_Hwang
Contributor II

When using s32ds software, generation does not work with the following error message.

please help.

Generator: ERROR: Error: LinStackCfg.npf line: 5 "bus_clock"- Syntax Error

 

Jackson_Hwang_1-1739275324871.png

 

 

标记 (1)
0 项奖励
回复
4 回复数

1,905 次查看
IsaulO
NXP Employee
NXP Employee

Hi @Jackson_Hwang ,

This is a known issue of LinStack in previous versions of SDK in S32DS for ARM, therefore we recommend working with the latest software versions, as previous versions may contain bugs that have been fixed in more recent releases. For example, S32DS 3.5 and RTD 2.0.0

BR,
IsaulO.

0 项奖励
回复

1,832 次查看
Jackson_Hwang
Contributor II

I am using the same version of SDK as the person who created the project: 

Jackson_Hwang_2-1739953683768.png

Jackson_Hwang_1-1739953639912.png

 

0 项奖励
回复

1,825 次查看
IsaulO
NXP Employee
NXP Employee

This SDK version (3.0.0) has this issue in the LinStack component (you can refer the following community thread: Solved: code generation error when using the lin_stack component with CPU_S32K142_48 in S32K1xx SDK ... ), which has been fixed in next versions, therefore you can use the SDK 3.0.3 or as workaround you can use the 100 pin variant, just paying attention to the available pins in the 48-pin package.

Note: We recommend working with the latest software versions. For example, S32DS 3.5 and RTD 2.0.0

BR,
IsaulO.

0 项奖励
回复

1,668 次查看
Jackson_Hwang
Contributor II

I'm trying to install the sdk3.0.3 update file in s32ds tools, but it fails to install with the following error.

items_could_not_be_installed.png

If it doesn't work online, I downloaded the update file from the site. Please tell me how to install it. Thank you.

Jackson_Hwang_0-1744626850887.png

 

标记 (1)
0 项奖励
回复