code generation error when using the lin_stack component with CPU_S32K142_48 in S32K1xx SDK RTM3.0.0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

code generation error when using the lin_stack component with CPU_S32K142_48 in S32K1xx SDK RTM3.0.0

Jump to solution
2,920 Views
enwei
NXP Employee
NXP Employee

Hello,

 

we met an issue of code generation when using the lin_stack component with CPU_S32K142_48 in S32K1xx SDK RTM3.0.0, it promts the following error, while there is no LinStackCfg.npf  in the project:

Description Resource Path Location Type
Generator: ERROR: Error: LinStackCfg.npf line: 5 "bus_clock"- Syntax Error... S32K142_LQFP48_LIN_Stack_Test_SDK_RTM3P0 lin_cfg Processor Expert Problem

pastedImage_4.png

PS: we tried the lin_stack component with Cpu_S32K142_100 package, it can generate the configuration codes normally. I attached the test project for your reference.

 

Can you help to verify and fix the bug?

 

Thanks~!

 

Best regard,

Enwei Hu(胡恩伟)

Labels (1)
Tags (3)
0 Kudos
Reply
1 Solution
2,783 Views
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Enwei Hu,

The SDK team confirmed that this behavior will be fixed in the next revision of the SDK. 

Best regards,

Victor

View solution in original post

0 Kudos
Reply
2 Replies
2,783 Views
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Enwei Hu, 

Thanks for catching this! I already reported this behavior to the corresponding team. 

Best regards, 

Victor 

0 Kudos
Reply
2,784 Views
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Enwei Hu,

The SDK team confirmed that this behavior will be fixed in the next revision of the SDK. 

Best regards,

Victor

0 Kudos
Reply