Ram_Ip_InitRamSection query

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Ram_Ip_InitRamSection query

958 Views
chalecampb
Contributor III

Deleting as this should have been on customer support portal

0 Kudos
Reply
2 Replies

896 Views
chalecampb
Contributor III

Moved to product support forum discussion

FYI this code is broken in WindRiver on S32K358

0 Kudos
Reply

927 Views
Nhi_Nguyen
NXP Employee
NXP Employee

Hi @chalecampb ,

I created 2 examples as below:

- Cast pointer that implement is similar with driver, in this case, inside pointer is 16U (or in driver it is RAM Section Size) or we can say address that pointer point to that used to be RAM Section Size. It is abnormal(no meaning when use pointer also) but from my point of view, have no problem here.

Nhi_Nguyen_0-1697168850926.png

- Pointer point to variable/structure that is as its definition about pointer. It is normal case.

Nhi_Nguyen_2-1697169422690.png

I agree that pointer used here without its meaning, but I didn't see any problem. Please let me know if I was wrong.

Best regards,

Nhi

 

0 Kudos
Reply