Ram_Ip_InitRamSection query

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Ram_Ip_InitRamSection query

1,602件の閲覧回数
chalecampb
Contributor III

Deleting as this should have been on customer support portal

0 件の賞賛
返信
2 返答(返信)

1,540件の閲覧回数
chalecampb
Contributor III

Moved to product support forum discussion

FYI this code is broken in WindRiver on S32K358

0 件の賞賛
返信

1,571件の閲覧回数
Nhi_Nguyen
NXP Employee
NXP Employee

Hi @chalecampb ,

I created 2 examples as below:

- Cast pointer that implement is similar with driver, in this case, inside pointer is 16U (or in driver it is RAM Section Size) or we can say address that pointer point to that used to be RAM Section Size. It is abnormal(no meaning when use pointer also) but from my point of view, have no problem here.

Nhi_Nguyen_0-1697168850926.png

- Pointer point to variable/structure that is as its definition about pointer. It is normal case.

Nhi_Nguyen_2-1697169422690.png

I agree that pointer used here without its meaning, but I didn't see any problem. Please let me know if I was wrong.

Best regards,

Nhi

 

0 件の賞賛
返信