Projects created by S32DS cannot be debugged

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Projects created by S32DS cannot be debugged

ソリューションへジャンプ
1,508件の閲覧回数
luhaiou_autolink
Contributor I

Ran into a very strange problem,

Projects created by S32DS cannot be debugged,

S32DS: 3.4

MCU :s32k314

RTD: 2.0.1

luhaiou_autolink_0-1709373776377.pngluhaiou_autolink_1-1709373818185.png

The simplest project that is created is directly debugged and cannot enter the main function normally

luhaiou_autolink_2-1709374139829.png

The newly created s32k344 and s32k312 projects can be debugged normally, only the s32K314 has an abnormality

0 件の賞賛
返信
1 解決策
1,464件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Sorry for the inconvenience we bring you!
This may be caused by RTD bug, please refer to the following discussion:
About linker_flash_s32k314.ld file created with S32DS
S32K314 burn directly to "HardFault Handler"
If your project has just started, it is recommended to use the latest S32K3 RTD.


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,465件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Sorry for the inconvenience we bring you!
This may be caused by RTD bug, please refer to the following discussion:
About linker_flash_s32k314.ld file created with S32DS
S32K314 burn directly to "HardFault Handler"
If your project has just started, it is recommended to use the latest S32K3 RTD.


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信