PINS_DRV_Init failed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PINS_DRV_Init failed

Jump to solution
1,882 Views
whale
Contributor III

Dear NXP Support Team,

I am encountering an issue while running the lpuart_echo_s32K144 example on a custom board. I would appreciate your assistance in resolving this problem.

Here's a detailed description of my setup and the steps I've taken:

Hardware: I have an S32K144evb-q100 evaluation board and a custom board (S32K144, 64-pin).
Software: I'm using S32DS 3.5 to create the lpuart_echo_s32K144 example with SDK version 4.0.2.

Steps Taken:

1. Step 1: I compiled and flashed the example onto the S32K144evb without any modifications. The example ran successfully on the EVB.
2. Step 2: I modified the project as follows:

  • Changed the package to LQFP64.
  • Remapped LPUART1 pins to PTC9 and PTC8.
    whale_0-1762846793005.png

     

  • Set LPUART1_CLK to 24MHz. My custom board does *not* have an external crystal oscillator; it uses FIRC as the clock source.
    whale_1-1762846828103.png

     

3. Step 3: After compilation, I attempted to debug the application on the custom board using J-Link.

Issue:

During debugging, the program enters an infinite loop at the following line of code:

whale_3-1762846978134.pngwhale_4-1762846994486.pngwhale_5-1762847066215.png

 

`uint32_t regValue = config->base->PCR[config->pinPortIdx];`

This leads to the execution of the `DefaultISR` function:

whale_2-1762846905056.png

Could you please advise on the potential cause of this issue and suggest possible solutions? I suspect the clock configuration or pin mapping might be the source of the problem.

Thank you for your time and assistance.

Sincerely,
Whale

Tags (1)
0 Kudos
Reply
1 Solution
1,835 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Please tell me your chip's maskset and part number. If it's an S32K144H, it only supports a maximum of 80MHz. If it's an S32K144U, it supports a maximum of HSRUN mode (112 MHz).

Please reconfigure the HSRUN clock by refer to the discussion in Creating New project : s32DS : Error clock not initializing

View solution in original post

0 Kudos
Reply
3 Replies
1,859 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

I modified the lpuart_echo_s32k144 according to your instructions in S32DS v3.4 + S32K1 SDK 4.0.3, but I didn't encounter this error on my S32K144EVB-Q100.

This error seems to indicate that the clock gate of the PORT is not enabled.

For your board that doesn't have onboard crystal, I suggest modifying the Clock tool configuration to disable SCG.SOSC.

Additionally, for S32K1 SDK 4.0.x, it is recommended to use CLOCK_DRV_Init. For details, please see: SDK problem in S32 Design Studio for ARM 2.2

  /* Initialize and configure clocks
   *     -    see clock manager component for details
   */
//  CLOCK_SYS_Init(g_clockManConfigsArr, CLOCK_MANAGER_CONFIG_CNT,
//                 g_clockManCallbacksArr, CLOCK_MANAGER_CALLBACK_CNT);
//  CLOCK_SYS_UpdateConfiguration(0U, CLOCK_MANAGER_POLICY_AGREEMENT);
  CLOCK_DRV_Init(&clockMan1_InitConfig0);
  /* Initialize pins
   *    -    See PinSettings component for more info
   */
  PINS_DRV_Init(NUM_OF_CONFIGURED_PINS0, g_pin_mux_InitConfigArr0);
By the way:
It is not recommended to install S32K1 SDK 4.0.x in S32DS v3.5 or v3.6. According to the currently available information, we don’t have any plan to integrate S32SDK S32K1XX 4.0.x into S32DS 3.5 or above version.
 

But we recommend to use the latest S32K1 RTD. The old SDK will not be updated to fix bugs.

Please download it by click Real-Time Drivers for S32K1 -> Automotive SW - S32K1_S32M24x - Real-Time Drivers for Cortex-M -> S32K1_S32M24X Real Time Drivers AUTOSAR R21-11 Version 3.0.0 ->  SW32K1_S32M24x_RTD_R21-11_3.0.0_D2503_DesignStudio_updatesite.zip
 


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply
1,841 Views
whale
Contributor III

Hi @Robin_Shen ,

Following your instructions, I modified the clock initialization function, and I also disabled SOSC in the clock configuration interface. However, when generating the code, the following error occurred:

whale_0-1762908385288.png

I'm not sure if this is the cause, but even after your modifications, the crash still occurs in the same place within PINS_Init.

How should I fix this?

Tags (1)
0 Kudos
Reply
1,836 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Please tell me your chip's maskset and part number. If it's an S32K144H, it only supports a maximum of 80MHz. If it's an S32K144U, it supports a maximum of HSRUN mode (112 MHz).

Please reconfigure the HSRUN clock by refer to the discussion in Creating New project : s32DS : Error clock not initializing

0 Kudos
Reply
%3CLINGO-SUB%20id%3D%22lingo-sub-2202518%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3EPINS_DRV_Init%20failed%3C%2FLINGO-SUB%3E%3CLINGO-BODY%20id%3D%22lingo-body-2202518%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%3CP%3EDear%20NXP%20Support%20Team%2C%3C%2FP%3E%3CP%3EI%20am%20encountering%20an%20issue%20while%20running%20the%20lpuart_echo_s32K144%20example%20on%20a%20custom%20board.%20I%20would%20appreciate%20your%20assistance%20in%20resolving%20this%20problem.%3C%2FP%3E%3CP%3EHere's%20a%20detailed%20description%20of%20my%20setup%20and%20the%20steps%20I've%20taken%3A%3C%2FP%3E%3CP%3E%3CSTRONG%3EHardware%3A%3C%2FSTRONG%3E%20I%20have%20an%20S32K144evb-q100%20evaluation%20board%20and%20a%20custom%20board%20(S32K144%2C%2064-pin).%3CBR%20%2F%3E%3CSTRONG%3ESoftware%3A%3C%2FSTRONG%3E%20I'm%20using%20S32DS%203.5%20to%20create%20the%20lpuart_echo_s32K144%20example%20with%20SDK%20version%204.0.2.%3C%2FP%3E%3CP%3E%3CSTRONG%3ESteps%20Taken%3A%3C%2FSTRONG%3E%3C%2FP%3E%3CP%3E1.%20%3CSTRONG%3EStep%201%3A%3C%2FSTRONG%3E%20I%20compiled%20and%20flashed%20the%20example%20onto%20the%20S32K144evb%20without%20any%20modifications.%20The%20example%20ran%20successfully%20on%20the%20EVB.%3CBR%20%2F%3E2.%20%3CSTRONG%3EStep%202%3A%3C%2FSTRONG%3E%20I%20modified%20the%20project%20as%20follows%3A%3C%2FP%3E%3CUL%3E%3CLI%3EChanged%20the%20package%20to%20LQFP64.%3C%2FLI%3E%3CLI%3ERemapped%20LPUART1%20pins%20to%20PTC9%20and%20PTC8.%3CBR%20%2F%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%20lia-image-align-inline%22%20image-alt%3D%22whale_0-1762846793005.png%22%20style%3D%22width%3A%20400px%3B%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22whale_0-1762846793005.png%22%20style%3D%22width%3A%20400px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F364881i5D7B776874A0B9E5%2Fimage-size%2Fmedium%3Fv%3Dv2%26amp%3Bpx%3D400%22%20role%3D%22button%22%20title%3D%22whale_0-1762846793005.png%22%20alt%3D%22whale_0-1762846793005.png%22%20%2F%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3CBR%20%2F%3E%3C%2FLI%3E%3CLI%3ESet%20LPUART1_CLK%20to%2024MHz.%20My%20custom%20board%20does%20*not*%20have%20an%20external%20crystal%20oscillator%3B%20it%20uses%20FIRC%20as%20the%20clock%20source.%3CBR%20%2F%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%20lia-image-align-inline%22%20image-alt%3D%22whale_1-1762846828103.png%22%20style%3D%22width%3A%20400px%3B%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22whale_1-1762846828103.png%22%20style%3D%22width%3A%20400px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F364882iA909D9DD47C12D47%2Fimage-size%2Fmedium%3Fv%3Dv2%26amp%3Bpx%3D400%22%20role%3D%22button%22%20title%3D%22whale_1-1762846828103.png%22%20alt%3D%22whale_1-1762846828103.png%22%20%2F%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3CBR%20%2F%3E%3C%2FLI%3E%3C%2FUL%3E%3CP%3E3.%20%3CSTRONG%3EStep%203%3A%3C%2FSTRONG%3E%20After%20compilation%2C%20I%20attempted%20to%20debug%20the%20application%20on%20the%20custom%20board%20using%20J-Link.%3C%2FP%3E%3CP%3E%3CSTRONG%3EIssue%3A%3C%2FSTRONG%3E%3C%2FP%3E%3CP%3EDuring%20debugging%2C%20the%20program%20enters%20an%20infinite%20loop%20at%20the%20following%20line%20of%20code%3A%3C%2FP%3E%3CP%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%20lia-image-align-inline%22%20image-alt%3D%22whale_3-1762846978134.png%22%20style%3D%22width%3A%20400px%3B%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22whale_3-1762846978134.png%22%20style%3D%22width%3A%20400px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F364884i2D7D6D56DB52FCD2%2Fimage-size%2Fmedium%3Fv%3Dv2%26amp%3Bpx%3D400%22%20role%3D%22button%22%20title%3D%22whale_3-1762846978134.png%22%20alt%3D%22whale_3-1762846978134.png%22%20%2F%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%20lia-image-align-inline%22%20image-alt%3D%22whale_4-1762846994486.png%22%20style%3D%22width%3A%20400px%3B%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22whale_4-1762846994486.png%22%20style%3D%22width%3A%20400px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F364885iD821AADE3B6D69BB%2Fimage-size%2Fmedium%3Fv%3Dv2%26amp%3Bpx%3D400%22%20role%3D%22button%22%20title%3D%22whale_4-1762846994486.png%22%20alt%3D%22whale_4-1762846994486.png%22%20%2F%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%20lia-image-align-inline%22%20image-alt%3D%22whale_5-1762847066215.png%22%20style%3D%22width%3A%20400px%3B%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22whale_5-1762847066215.png%22%20style%3D%22width%3A%20400px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F364886i135EB4CBCE013EF1%2Fimage-size%2Fmedium%3Fv%3Dv2%26amp%3Bpx%3D400%22%20role%3D%22button%22%20title%3D%22whale_5-1762847066215.png%22%20alt%3D%22whale_5-1762847066215.png%22%20%2F%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FP%3E%3CBR%20%2F%3E%3CP%3E%60%3CSTRONG%3Euint32_t%20regValue%20%3D%20config-%26gt%3Bbase-%26gt%3BPCR%5Bconfig-%26gt%3BpinPortIdx%5D%3B%3C%2FSTRONG%3E%60%3C%2FP%3E%3CP%3EThis%20leads%20to%20the%20execution%20of%20the%20%60DefaultISR%60%20function%3A%3C%2FP%3E%3CP%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%20lia-image-align-inline%22%20image-alt%3D%22whale_2-1762846905056.png%22%20style%3D%22width%3A%20400px%3B%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22whale_2-1762846905056.png%22%20style%3D%22width%3A%20319px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F364883i698D4C9324E4BA0A%2Fimage-size%2Fmedium%3Fv%3Dv2%26amp%3Bpx%3D400%22%20role%3D%22button%22%20title%3D%22whale_2-1762846905056.png%22%20alt%3D%22whale_2-1762846905056.png%22%20%2F%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FP%3E%3CP%3ECould%20you%20please%20advise%20on%20the%20potential%20cause%20of%20this%20issue%20and%20suggest%20possible%20solutions%3F%20I%20suspect%20the%20clock%20configuration%20or%20pin%20mapping%20might%20be%20the%20source%20of%20the%20problem.%3C%2FP%3E%3CP%3EThank%20you%20for%20your%20time%20and%20assistance.%3C%2FP%3E%3CP%3ESincerely%2C%3CBR%20%2F%3EWhale%3C%2FP%3E%3C%2FLINGO-BODY%3E%3CLINGO-SUB%20id%3D%22lingo-sub-2203051%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%20translate%3D%22no%22%3ERe%3A%20PINS_DRV_Init%20failed%3C%2FLINGO-SUB%3E%3CLINGO-BODY%20id%3D%22lingo-body-2203051%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%3CP%3EPlease%20tell%20me%20your%20chip's%20maskset%20and%20part%20number.%20If%20it's%20an%20S32K144%3CSTRONG%3EH%3C%2FSTRONG%3E%2C%20it%20only%20supports%20a%20maximum%20of%20%3CSTRONG%3E80%3C%2FSTRONG%3EMHz.%20If%20it's%20an%20S32K144%3CSTRONG%3EU%3C%2FSTRONG%3E%2C%20it%20supports%20a%20maximum%20of%20HSRUN%20mode%20(%3CSTRONG%3E112%3C%2FSTRONG%3E%20MHz).%3C%2FP%3E%0A%3CP%3EPlease%20reconfigure%20the%20HSRUN%20clock%20by%20refer%20to%20the%20discussion%20in%26nbsp%3B%3CA%20href%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2FS32K%2FCreating-New-project-s32DS-Error-clock-not-initializing%2Ftd-p%2F1331744%22%20target%3D%22_self%22%3ECreating%20New%20project%20%3A%20s32DS%20%3A%20Error%20clock%20not%20initializing%3C%2FA%3E%3C%2FP%3E%3C%2FLINGO-BODY%3E%3CLINGO-SUB%20id%3D%22lingo-sub-2203032%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%20translate%3D%22no%22%3ERe%3A%20PINS_DRV_Init%20failed%3C%2FLINGO-SUB%3E%3CLINGO-BODY%20id%3D%22lingo-body-2203032%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%3CP%3EHi%26nbsp%3B%3CA%20href%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fuser%2Fviewprofilepage%2Fuser-id%2F57959%22%20target%3D%22_blank%22%3E%40Robin_Shen%3C%2FA%3E%26nbsp%3B%2C%3C%2FP%3E%3CP%3E%3CSPAN%3EFollowing%20your%20instructions%2C%20I%20modified%20the%20clock%20initialization%20function%2C%20and%20I%20also%20disabled%20SOSC%20in%20the%20clock%20configuration%20interface.%20However%2C%20when%20generating%20the%20code%2C%20the%20following%20error%20occurred%3A%3C%2FSPAN%3E%3C%2FP%3E%3CP%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%20lia-image-align-inline%22%20image-alt%3D%22whale_0-1762908385288.png%22%20style%3D%22width%3A%20400px%3B%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22whale_0-1762908385288.png%22%20style%3D%22width%3A%20400px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F365033i91ED31D2DA4948B2%2Fimage-size%2Fmedium%3Fv%3Dv2%26amp%3Bpx%3D400%22%20role%3D%22button%22%20title%3D%22whale_0-1762908385288.png%22%20alt%3D%22whale_0-1762908385288.png%22%20%2F%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FP%3E%3CP%3E%3CSPAN%3EI'm%20not%20sure%20if%20this%20is%20the%20cause%2C%20but%20even%20after%20your%20modifications%2C%20the%20crash%20still%20occurs%20in%20the%20same%20place%20within%20PINS_Init.%3C%2FSPAN%3E%3C%2FP%3E%3CP%3E%3CSPAN%3EHow%20should%20I%20fix%20this%3F%3C%2FSPAN%3E%3C%2FP%3E%3C%2FLINGO-BODY%3E%3CLINGO-SUB%20id%3D%22lingo-sub-2202611%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%20translate%3D%22no%22%3ERe%3A%20PINS_DRV_Init%20failed%3C%2FLINGO-SUB%3E%3CLINGO-BODY%20id%3D%22lingo-body-2202611%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%3CP%3EHi%3C%2FP%3E%0A%3CP%3EI%20modified%20the%20%3CSTRONG%3Elpuart_echo_s32k144%3C%2FSTRONG%3E%20according%20to%20your%20instructions%20in%20S32DS%20v3.4%20%2B%20S32K1%20SDK%20%3CSTRONG%3E4.0.3%3C%2FSTRONG%3E%2C%20but%20I%20didn't%20encounter%20this%20error%20on%20my%20S32K144EVB-Q100.%3C%2FP%3E%0A%3CP%3EThis%20error%20seems%20to%20indicate%20that%20the%20clock%20gate%20of%20the%20PORT%20is%20not%20enabled.%3C%2FP%3E%0A%3CP%3EFor%20your%20board%20that%20doesn't%20have%20onboard%20crystal%2C%20I%20suggest%20modifying%20the%20%3CSTRONG%3E%3CEM%3EClock%20tool%3C%2FEM%3E%3C%2FSTRONG%3E%20configuration%20to%20disable%20%3CSTRONG%3ESCG.SOSC%3C%2FSTRONG%3E.%3C%2FP%3E%0A%3CP%3EAdditionally%2C%20for%20S32K1%20SDK%204.0.x%2C%20it%20is%20recommended%20to%20use%20%3CSTRONG%3ECLOCK_DRV_Init%3C%2FSTRONG%3E.%20For%20details%2C%20please%20see%3A%20%3CA%20href%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2FS32-SDK%2FSDK-problem-in-S32-Design-Studio-for-ARM-2-2%2Fm-p%2F986190%22%20target%3D%22_self%22%3ESDK%20problem%20in%20S32%20Design%20Studio%20for%20ARM%202.2%3C%2FA%3E%3C%2FP%3E%0A%3CPRE%20class%3D%22lia-code-sample%20language-markup%22%3E%3CCODE%3E%20%20%2F*%20Initialize%20and%20configure%20clocks%0A%20%20%20*%20%20%20%20%20-%20%20%20%20see%20clock%20manager%20component%20for%20details%0A%20%20%20*%2F%0A%2F%2F%20%20CLOCK_SYS_Init(g_clockManConfigsArr%2C%20CLOCK_MANAGER_CONFIG_CNT%2C%0A%2F%2F%20%20%20%20%20%20%20%20%20%20%20%20%20%20%20%20%20g_clockManCallbacksArr%2C%20CLOCK_MANAGER_CALLBACK_CNT)%3B%0A%2F%2F%20%20CLOCK_SYS_UpdateConfiguration(0U%2C%20CLOCK_MANAGER_POLICY_AGREEMENT)%3B%0A%20%20CLOCK_DRV_Init(%26amp%3BclockMan1_InitConfig0)%3B%0A%20%20%2F*%20Initialize%20pins%0A%20%20%20*%20%20%20%20-%20%20%20%20See%20PinSettings%20component%20for%20more%20info%0A%20%20%20*%2F%0A%20%20PINS_DRV_Init(NUM_OF_CONFIGURED_PINS0%2C%20g_pin_mux_InitConfigArr0)%3B%3C%2FCODE%3E%3C%2FPRE%3E%0A%3CDIV%3EBy%20the%20way%3A%3C%2FDIV%3E%0A%3CDIV%3EIt%20is%20not%20recommended%20to%20install%20S32K1%26nbsp%3BSDK%204.0.x%26nbsp%3Bin%20S32DS%26nbsp%3Bv3.5%20or%20v3.6.%26nbsp%3BAccording%20to%20the%20currently%20available%20information%2C%20we%20don%E2%80%99t%20have%20any%20plan%20to%20integrate%20S32SDK%20S32K1XX%204.0.x%20into%20S32DS%203.5%20or%20above%20version.%3C%2FDIV%3E%0A%3CDIV%3E%26nbsp%3B%3C%2FDIV%3E%0A%3CP%3E%3CSPAN%3EBut%20we%20recommend%20to%20use%20the%20latest%20S32K1%20RTD.%20The%20old%20SDK%20will%20not%20be%20updated%20to%20fix%20bugs.%3C%2FSPAN%3E%3C%2FP%3E%0A%3CDIV%3EPlease%20download%20it%20by%20click%26nbsp%3B%3CA%20href%3D%22https%3A%2F%2Fwww.nxp.com%2Fwebapp%2Fswlicensing%2Fsso%2FdownloadSoftware.sp%3Fcatid%3DSW32K1-RTD44-D%22%20target%3D%22_blank%22%20rel%3D%22noopener%20nofollow%20noreferrer%22%20shape%3D%22rect%22%3EReal-Time%20Drivers%20for%20S32K1%3C%2FA%3E%26nbsp%3B-%26gt%3B%20Automotive%20SW%20-%20S32K1_S32M24x%20-%20Real-Time%20Drivers%20for%20Cortex-M%20-%26gt%3B%20S32K1_S32M24X%20Real%20Time%20Drivers%20AUTOSAR%20R21-11%20Version%203.0.0%20-%26gt%3B%20%26nbsp%3BSW32K1_S32M24x_RTD_R21-11_3.0.0_D2503_DesignStudio_updatesite.zip%3C%2FDIV%3E%0A%3CDIV%3E%26nbsp%3B%3C%2FDIV%3E%0A%3CDIV%3EThen%20install%20it%20in%26nbsp%3B%3CA%20href%3D%22https%3A%2F%2Fwww.nxp.com%2Fwebapp%2Fswlicensing%2Fsso%2FdownloadSoftware.sp%3Fcatid%3DS32DS-3-6%22%20target%3D%22_blank%22%20rel%3D%22noopener%20nofollow%20noreferrer%22%20shape%3D%22rect%22%3ES32DS%20v3.6.1%26nbsp%3B%3C%2FA%3Eby%20refer%20to%26nbsp%3B%3CA%20href%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2FS32-Design-Studio-Knowledge-Base%2FHOWTO-S32-Design-Studio-Offline-Install-of-Extensions-and%2Fta-p%2F1126424%22%20target%3D%22_blank%22%20shape%3D%22rect%22%3Ehttps%3A%2F%2Fcommunity.nxp.com%2Ft5%2FS32-Design-Studio-Knowledge-Base%2FHOWTO-S32-Design-Studio-Offline-Install-of-Extensions-and%2Fta-p%2F1126424%3C%2FA%3E%3C%2FDIV%3E%0A%3CDIV%3E%0A%3CP%3E%3CBR%20%2F%3EBest%20Regards%2C%3CBR%20%2F%3ERobin%3CBR%20%2F%3E-------------------------------------------------------------------------------%3CBR%20%2F%3ENote%3A%3CBR%20%2F%3E-%20If%20this%20post%20answers%20your%20question%2C%20please%20click%20the%20%22ACCEPT%20AS%20SOLUTION%22%20button.%20Thank%20you!%3C%2FP%3E%0A%3CP%3E-%20We%20are%20following%20threads%20for%207%20weeks%20after%20the%20last%20post%2C%20later%20replies%20are%20ignored%3CBR%20%2F%3EPlease%20open%20a%20new%20thread%20and%20refer%20to%20the%20closed%20one%2C%20if%20you%20have%20a%20related%20question%20at%20a%20later%20point%20in%20time.%3CBR%20%2F%3E-------------------------------------------------------------------------------%3C%2FP%3E%0A%3C%2FDIV%3E%3C%2FLINGO-BODY%3E