OpenBus

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
6,191件の閲覧回数
geoff_roy
Contributor II

Is Openbus.exe compatible with Vector 1630A CAN device?? I don-t have a P-CAN device with me, but has a Vector 1630A CAN device. Will that be a challenge. @dianabatrlova 

タグ(3)
0 件の賞賛
返信
1 解決策
6,165件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Geoff,

I expect that any PCAN-USB... can be used but I will ask to be sure.

Regards,

Lukas

 

元の投稿で解決策を見る

0 件の賞賛
返信
7 返答(返信)
6,029件の閲覧回数
HayZam
Contributor II

Hello,
How should the physical connection be for using OpenBus.exe with LIN  and S32K116EVB?

Is connecting pin 7 (LIN) and pin 3 (GND) to the EVB enough?
Is any extra configuration required to use this tool?

Regards,
HayZam

0 件の賞賛
返信
6,181件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

I'm afraid that P-CAN is currently the only option.

Regards,

Lukas

 

0 件の賞賛
返信
6,172件の閲覧回数
geoff_roy
Contributor II

Hi Lukas,

Could you please help me with the version or specific device name to be purchased for easy use of Openbus software.

 

Thanks and Regards,

Geoff

0 件の賞賛
返信
6,134件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Geoff,

I was told that all PCAN USB devices should be detected and identified by OpenBus SW.

It was tested with basic PCAN-USB.

Hope this helps.

Regards,

Lukas

 

0 件の賞賛
返信
6,166件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Geoff,

I expect that any PCAN-USB... can be used but I will ask to be sure.

Regards,

Lukas

 

0 件の賞賛
返信
5,899件の閲覧回数
DBD
Contributor I

Hi Lukaszadrapa

I wan to use OpenBus but i don 't have Peak can adapter, i have a other USB-CAN adapter. so how to modify OpenBus to compatible other adapter. thanks

タグ(1)
0 件の賞賛
返信
6,107件の閲覧回数
geoff_roy
Contributor II

Thanks for your input.

0 件の賞賛
返信