Not able to partition flash of S32K144 using example project

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Not able to partition flash of S32K144 using example project

Jump to solution
1,976 Views
emb02
Contributor IV

Hi,

I'm using flash_partitioning_s32k144 example project for testing but not able to partition Flash.

-> FLASH_DRV_CommandSequence() at flash_driver.c:290 0x1fff85e2

After this function program is going into DefaultISR while debugging.

S32K eeprom error.png

I'm using internal clock of S32K144 and modified clock setting as per my requirement (internal clock).
I'm attaching my project for reference. Please guide me further.

Regards,

EMB02

0 Kudos
Reply
1 Solution
1,903 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

As far as I remembered, we don’t have any plan to integrate S32SDK S32K1XX 4.0.3 into S32DS 3.5 or above version.

View solution in original post

0 Kudos
Reply
5 Replies
1,931 Views
emb02
Contributor IV

Hi,

Thank you for your response.

I am not able to install - S32K1 SDK RTM 4.0.3. There is no option for installing SDK 4.0.3.

SDK.png

Can you please guide me further to install SDK.

 

Regards,

EMB02

0 Kudos
Reply
1,917 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

S32K1 SDK RTM 4.0.3 is not available in S32DS v3.5, please install it in S32DS v3.4.
Sorry for the inconvenience we bring you!

0 Kudos
Reply
1,907 Views
emb02
Contributor IV
Hi,

Can S32DS v3.5 will be updated with SDK RTM 4.0.3 in upcoming days?

Regards,
EMB02
0 Kudos
Reply
1,904 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

As far as I remembered, we don’t have any plan to integrate S32SDK S32K1XX 4.0.3 into S32DS 3.5 or above version.

0 Kudos
Reply
1,952 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi EMB02,

Please use S32K1 SDK RTM 4.0.3 with S32DS v3.4. From S32SDK_for_S32K1xx_RTM_4.0.2_ReleaseNotes.pdf you can see that a Flash issue has been fixed: Fixed issue of flash component: generate callback with NULL value.

List of fixed issues from S32K1xx RTM 4.0.1 generate callback with NULL value.jpg


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply