Hi,
I'm using flash_partitioning_s32k144 example project for testing but not able to partition Flash.
-> FLASH_DRV_CommandSequence() at flash_driver.c:290 0x1fff85e2
After this function program is going into DefaultISR while debugging.
I'm using internal clock of S32K144 and modified clock setting as per my requirement (internal clock).
I'm attaching my project for reference. Please guide me further.
Regards,
EMB02
Solved! Go to Solution.
As far as I remembered, we don’t have any plan to integrate S32SDK S32K1XX 4.0.3 into S32DS 3.5 or above version.
Hi,
Thank you for your response.
I am not able to install - S32K1 SDK RTM 4.0.3. There is no option for installing SDK 4.0.3.
Can you please guide me further to install SDK.
Regards,
EMB02
S32K1 SDK RTM 4.0.3 is not available in S32DS v3.5, please install it in S32DS v3.4.
Sorry for the inconvenience we bring you!
As far as I remembered, we don’t have any plan to integrate S32SDK S32K1XX 4.0.3 into S32DS 3.5 or above version.
Hi EMB02,
Please use S32K1 SDK RTM 4.0.3 with S32DS v3.4. From S32SDK_for_S32K1xx_RTM_4.0.2_ReleaseNotes.pdf you can see that a Flash issue has been fixed: Fixed issue of flash component: generate callback with NULL value.
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------