Need Pin Clarification for Part number S32K342NHT0MPBSR

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Need Pin Clarification for Part number S32K342NHT0MPBSR

1,108 次查看
Divyashree1
Contributor I

Hi Team,

How the pin PTE13(11) output should be defined, Specifically the min and max output voltages. Also define the maximum current capability of this pin.

0 项奖励
回复
1 回复

1,082 次查看
Senlent
NXP TechSupport
NXP TechSupport

Hi@Divyashree1

there is no Max output high current parameter.

the output voltage should be euqal to VDD_HV_A and the Min output high current should be no less than 1.6 mA.

 

Senlent_2-1681112716106.png

 

0 项奖励
回复