Need Pin Clarification for Part number S32K342NHT0MPBSR

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Need Pin Clarification for Part number S32K342NHT0MPBSR

1,090 Views
Divyashree1
Contributor I

Hi Team,

How the pin PTE13(11) output should be defined, Specifically the min and max output voltages. Also define the maximum current capability of this pin.

0 Kudos
Reply
1 Reply

1,064 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@Divyashree1

there is no Max output high current parameter.

the output voltage should be euqal to VDD_HV_A and the Min output high current should be no less than 1.6 mA.

 

Senlent_2-1681112716106.png

 

0 Kudos
Reply