Multiple versions of S32DS on the same PC?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Multiple versions of S32DS on the same PC?

ソリューションへジャンプ
1,136件の閲覧回数
davorin_mista
Contributor I

Is it safe to have S32DS v1.3 and 2018.R1 installed on the same PC? 

Thanks,
Davorin

0 件の賞賛
返信
1 解決策
1,126件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

Yes, it is. I have also installed multiple S32DS versions and everything works as expected.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,127件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

Yes, it is. I have also installed multiple S32DS versions and everything works as expected.

0 件の賞賛
返信
1,117件の閲覧回数
davorin_mista
Contributor I

I strongly suspect that my problems detecting the OpenSDA debug port were caused by installing those two versions in parallel. Uninstalled both, uninstalled the drivers and then installed only 2018.R1 fixed my problem

0 件の賞賛
返信