Multiple versions of S32DS on the same PC?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Multiple versions of S32DS on the same PC?

跳至解决方案
1,130 次查看
davorin_mista
Contributor I

Is it safe to have S32DS v1.3 and 2018.R1 installed on the same PC? 

Thanks,
Davorin

0 项奖励
回复
1 解答
1,120 次查看
davidtosenovjan
NXP TechSupport
NXP TechSupport

Yes, it is. I have also installed multiple S32DS versions and everything works as expected.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,121 次查看
davidtosenovjan
NXP TechSupport
NXP TechSupport

Yes, it is. I have also installed multiple S32DS versions and everything works as expected.

0 项奖励
回复
1,111 次查看
davorin_mista
Contributor I

I strongly suspect that my problems detecting the OpenSDA debug port were caused by installing those two versions in parallel. Uninstalled both, uninstalled the drivers and then installed only 2018.R1 fixed my problem

0 项奖励
回复