Multiple versions of S32DS on the same PC?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multiple versions of S32DS on the same PC?

Jump to solution
1,134 Views
davorin_mista
Contributor I

Is it safe to have S32DS v1.3 and 2018.R1 installed on the same PC? 

Thanks,
Davorin

0 Kudos
Reply
1 Solution
1,124 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Yes, it is. I have also installed multiple S32DS versions and everything works as expected.

View solution in original post

0 Kudos
Reply
2 Replies
1,125 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Yes, it is. I have also installed multiple S32DS versions and everything works as expected.

0 Kudos
Reply
1,115 Views
davorin_mista
Contributor I

I strongly suspect that my problems detecting the OpenSDA debug port were caused by installing those two versions in parallel. Uninstalled both, uninstalled the drivers and then installed only 2018.R1 fixed my problem

0 Kudos
Reply