Missing Directory in an Example code

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Missing Directory in an Example code

跳至解决方案
2,366 次查看
akhilranga
Contributor IV

Hello there. I am new in this space. And trying to find my ropes here. I am following a s32k144 cookbook to get familar to the s32 design studio application and s32k144 board. And i have encountered the following error. Can any suggest me, how to resolve this. Is there any way i can add that missing file

Screenshot (118).png

Thank in advance. Would really appriciate it

#s32k144

 

标记 (1)
0 项奖励
回复
1 解答
2,360 次查看
Senlent
NXP TechSupport
NXP TechSupport

Hi@akhilranga

 Have you added the clocks_and_modes.c & clock_and_modes.h to your project?

Senlent_0-1657677006013.png

if no, you need to add these file to your project.

if yes,you may forget to add these file path,you can take a look at this post.

https://community.nxp.com/t5/S32K/S32K-S32DS-project-name-path-and-build-problem/td-p/1260029 

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,361 次查看
Senlent
NXP TechSupport
NXP TechSupport

Hi@akhilranga

 Have you added the clocks_and_modes.c & clock_and_modes.h to your project?

Senlent_0-1657677006013.png

if no, you need to add these file to your project.

if yes,you may forget to add these file path,you can take a look at this post.

https://community.nxp.com/t5/S32K/S32K-S32DS-project-name-path-and-build-problem/td-p/1260029 

0 项奖励
回复
2,355 次查看
akhilranga
Contributor IV

Hello thee,

I didn't add them in my project. Hoping those files are available in NXP resources. May i know the process to add them in my project.

Thank You 

0 项奖励
回复