Mcl_Trgmux_Group

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,195件の閲覧回数
gadilinga
Contributor III

Hi,

Mcl_Trigger Mux Group was there  in that Group From TRGMUX_IP_INPUT_EMIOS1_IPP_ 0 to 15 ,22 and 23. If i want Select the Trgmux_Logic_trigger Hardware Input of emios channel to Hardware Out of Lcu0. currently Im using Emios Channel number 21,22. So which Trgmux Logic Trigger Input i need to select for channel num 21 and 22.

gadilinga_0-1725004222308.png

 

0 件の賞賛
返信
1 解決策
1,136件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@gadilinga

"But That Channel Suggested NXP only."

what does it mean? Can you show me a screenshot?

元の投稿で解決策を見る

0 件の賞賛
返信
6 返答(返信)
1,181件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@gadilinga

Actually you can see what channel can be used in TRGMUX.

Senlent_0-1725007983445.png

and EMIOS_0_IPP_DO_eMIOS_CH[21] can not be used for TRGMUX input.

 

0 件の賞賛
返信
1,177件の閲覧回数
gadilinga
Contributor III
Hi @Senlent,
Currently I'm using Emios0_Ch[0],Emios0_Ch[1], Emios1_Ch[6],Emios1_Ch[7],Emios1_Ch[21 And Emios1_Ch[22] these 6 channel using For Pwm.
i need Each channel Emios Input Trigger Mux AS for NXP Application:AN13767 :S32K344 module interconnection Diagrams. for Got 5 channels But 21 I didn't get So As u mention Above comment. what was Solution for This Problem.
0 件の賞賛
返信
1,173件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@gadilinga

This is not a problem. eMIOS's CH21 cannot be used as the input of TRGMUX. What you can do is to change other channels.

0 件の賞賛
返信
1,170件の閲覧回数
gadilinga
Contributor III
Hi @Senlent,
But That Channel Suggested NXP only.
0 件の賞賛
返信
1,137件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@gadilinga

"But That Channel Suggested NXP only."

what does it mean? Can you show me a screenshot?

0 件の賞賛
返信
1,132件の閲覧回数
gadilinga
Contributor III
Hi @Senlent,
Thank u For Ur Quick Response towards the the Solution. It doesn't mean that NXP , It mean Each Emios Instance Have 24 Channels, So if U see the TRGMUX Connectivity 0 to 15,22,and 23 channels only in TRGMUX logic Group. If i use Emios Out of 23 channels why 16 to 21 channels Input not Available in that Option. .
0 件の賞賛
返信