Hi,
Mcl_Trigger Mux Group was there in that Group From TRGMUX_IP_INPUT_EMIOS1_IPP_ 0 to 15 ,22 and 23. If i want Select the Trgmux_Logic_trigger Hardware Input of emios channel to Hardware Out of Lcu0. currently Im using Emios Channel number 21,22. So which Trgmux Logic Trigger Input i need to select for channel num 21 and 22.
解決済! 解決策の投稿を見る。
"But That Channel Suggested NXP only."
what does it mean? Can you show me a screenshot?
Actually you can see what channel can be used in TRGMUX.
and EMIOS_0_IPP_DO_eMIOS_CH[21] can not be used for TRGMUX input.
This is not a problem. eMIOS's CH21 cannot be used as the input of TRGMUX. What you can do is to change other channels.
"But That Channel Suggested NXP only."
what does it mean? Can you show me a screenshot?