MCAL CAN plugin generation error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCAL CAN plugin generation error

ソリューションへジャンプ
4,662件の閲覧回数
talha_uyar
Contributor III

Hi, I was trying to generate the .cfg files for the Can plugin using Tresos. I get the following error and could not understand the reason. I am quite new at this so the issue might be trivial. 

All answers are appreciated,

M. Talha Uyar 

Error:

Parsing file "C:\EB\tresos\..\..\NXP\AUTOSAR\S32K14X_MCAL4_3_RTM_HF2_1_0_1\eclipse\plugins\Can_TS_T40D2M10I1R0/generate_PC/include/Can_Cfg.h (signed)", line "1366"
The XPath-expression "node:ref(CanGeneral/CanOsCounterRef)" caused an error: (1844) No node found for path ""

Edit: Ok, I see that I haven't set a Reference at the Can Counter Ref. section. So my question is how do I set up a counter to be referenced by the CAN plugin?

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
4,497件の閲覧回数
hungnguyenphi
NXP Employee
NXP Employee

Hello Muhammet Uyar ,

User need to add module OS to have the Reference for the "Can Counter Ref".

If you don't want to use OS, please check to the "Can define loop as cycle* " to use "Can Timeout Duration (in Number of loops) (1 -> 65535)" instead of "Can Counter Ref".

元の投稿で解決策を見る

1 返信
4,498件の閲覧回数
hungnguyenphi
NXP Employee
NXP Employee

Hello Muhammet Uyar ,

User need to add module OS to have the Reference for the "Can Counter Ref".

If you don't want to use OS, please check to the "Can define loop as cycle* " to use "Can Timeout Duration (in Number of loops) (1 -> 65535)" instead of "Can Counter Ref".