About S32KXXX MCU function safety

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About S32KXXX MCU function safety

1,809 Views
taiguo_han
Contributor I

From the below picture I found S32K116 MCU, some are labeled as "ISO26262" and some are labeled as "No" 

but for the "ASIL Certification" tab, all the MCU labeled "up to ASIL-B"  

pastedImage_1.png

I don't know if all of these MCU could meet the ASIL B level, or only those labeled "ISO 26262" in the "SafetyAssure Functional Safety" tab can reach ASIL B level? 

If someone could help me?

0 Kudos
Reply
1 Reply

1,721 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello [email protected],

The page is going to be fixed.

All the S32K1xx parts are ISO 26262 compliant up to ASIL-B.

Thank you for pointing it out.

Regards,

Daniel

0 Kudos
Reply