LPSPI_IP_BUSY state while transmitting data from Lpspi_Ip_AsyncTransmit() function

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPSPI_IP_BUSY state while transmitting data from Lpspi_Ip_AsyncTransmit() function

Jump to solution
1,758 Views
prasadrashinkar
Contributor II

We have  an issue With S32k44,

configured LPSPI using EB tresos and tried to transmit data using Lpspi_Ip_AsyncTransmit()

call gets executed once Other calls are rejected because the drivers stay in the LPSPI_IP_BUSY state.

Can you please share an Example project of S32K344(with EB tresos configuration)

for Lpspi_Ip_AsyncTransmit(); using DMA?

#S32K344

 

0 Kudos
Reply
1 Solution
1,644 Views
prasadrashinkar
Contributor II

Thanks Petr

using this example I can use SPI, and the issue is resolved 

View solution in original post

0 Kudos
Reply
2 Replies
1,741 Views
PetrS
NXP TechSupport
NXP TechSupport
0 Kudos
Reply
1,645 Views
prasadrashinkar
Contributor II

Thanks Petr

using this example I can use SPI, and the issue is resolved 

0 Kudos
Reply