LDF LIN stack generate lin cfg code miss

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LDF LIN stack generate lin cfg code miss

ソリューションへジャンプ
3,668件の閲覧回数
liuxing_hu
Contributor III

liuxing_hu_0-1629855169086.pngliuxing_hu_0-1629855169086.png

as the picture show, there are 2 slave frames(LIN_Slave_SWSR_SWIT and LIN_Slave_SWSL_SWIT) in LDF file, but when reload LDF file, and generate, only the code of LIN_Slave_SWSL_SWIT  generate in lin_cfg.h, I can'r find the code of LIN_Slave_SWSR_SWIT in lin_cfg.h, does I miss something to config?

0 件の賞賛
返信
1 解決策
3,654件の閲覧回数
hungnguyenphi
NXP Employee
NXP Employee

Hello @liuxing_hu ,

 

One interface in the MCU will represent just one node in the Lin Network which is described in the LDF file. Then the LinStack just generated the code for the corresponding node.

hungnguyenphi_1-1629968334568.pnghungnguyenphi_1-1629968334568.png

 

Best regards,

Hung

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
3,553件の閲覧回数
gaowei
Contributor I

我的S32DS 出现lin ldf文件不能用通过Generated方式输出内容到lin_cfg.c 和.H. ;lin_cfg.c文件中内容没有ldf的相关内容。请问您觉得可能是哪里出了问题?

0 件の賞賛
返信
3,655件の閲覧回数
hungnguyenphi
NXP Employee
NXP Employee

Hello @liuxing_hu ,

 

One interface in the MCU will represent just one node in the Lin Network which is described in the LDF file. Then the LinStack just generated the code for the corresponding node.

hungnguyenphi_1-1629968334568.pnghungnguyenphi_1-1629968334568.png

 

Best regards,

Hung

0 件の賞賛
返信