LDF LIN stack generate lin cfg code miss

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LDF LIN stack generate lin cfg code miss

Jump to solution
3,631 Views
liuxing_hu
Contributor III

liuxing_hu_0-1629855169086.pngliuxing_hu_0-1629855169086.png

as the picture show, there are 2 slave frames(LIN_Slave_SWSR_SWIT and LIN_Slave_SWSL_SWIT) in LDF file, but when reload LDF file, and generate, only the code of LIN_Slave_SWSL_SWIT  generate in lin_cfg.h, I can'r find the code of LIN_Slave_SWSR_SWIT in lin_cfg.h, does I miss something to config?

0 Kudos
Reply
1 Solution
3,617 Views
hungnguyenphi
NXP Employee
NXP Employee

Hello @liuxing_hu ,

 

One interface in the MCU will represent just one node in the Lin Network which is described in the LDF file. Then the LinStack just generated the code for the corresponding node.

hungnguyenphi_1-1629968334568.pnghungnguyenphi_1-1629968334568.png

 

Best regards,

Hung

View solution in original post

0 Kudos
Reply
2 Replies
3,516 Views
gaowei
Contributor I

我的S32DS 出现lin ldf文件不能用通过Generated方式输出内容到lin_cfg.c 和.H. ;lin_cfg.c文件中内容没有ldf的相关内容。请问您觉得可能是哪里出了问题?

0 Kudos
Reply
3,618 Views
hungnguyenphi
NXP Employee
NXP Employee

Hello @liuxing_hu ,

 

One interface in the MCU will represent just one node in the Lin Network which is described in the LDF file. Then the LinStack just generated the code for the corresponding node.

hungnguyenphi_1-1629968334568.pnghungnguyenphi_1-1629968334568.png

 

Best regards,

Hung

0 Kudos
Reply