ISELED without EVB

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

ISELED without EVB

跳至解决方案
1,889 次查看
cristian20a
Contributor I

Hi all,

I have tried the S32K144-EVB with ISELED and now I would like to develop my own PCB and try the proper MCU with an integrated iseled interface. But I wanna know if I have to consider other things. For example, when using the evb and SDK it has a maximum number of configurations and then you have to reflash, with the proper MCUs I suppose that there is not a limit, right? is there anything else to consider?

E.g of MCUs with ISELED: FS32K116LIT0VFMT, FS32K118LIT0VLFT, etc.

Thank you,

Cristian

标记 (5)
0 项奖励
回复
1 解答
1,873 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hi Cristian,

Yes, as you can see in FACT SHEET S32K ISELED

https://www.nxp.com/docs/en/fact-sheet/S32K-ISELED-FS.pdf

For production, developers should order one of the S32K ISELED part numbers
below which include the full production license with unlimited driver functionality.

 

BR, Daniel

 

在原帖中查看解决方案

1 回复
1,874 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hi Cristian,

Yes, as you can see in FACT SHEET S32K ISELED

https://www.nxp.com/docs/en/fact-sheet/S32K-ISELED-FS.pdf

For production, developers should order one of the S32K ISELED part numbers
below which include the full production license with unlimited driver functionality.

 

BR, Daniel