ISELED without EVB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,905件の閲覧回数
cristian20a
Contributor I

Hi all,

I have tried the S32K144-EVB with ISELED and now I would like to develop my own PCB and try the proper MCU with an integrated iseled interface. But I wanna know if I have to consider other things. For example, when using the evb and SDK it has a maximum number of configurations and then you have to reflash, with the proper MCUs I suppose that there is not a limit, right? is there anything else to consider?

E.g of MCUs with ISELED: FS32K116LIT0VFMT, FS32K118LIT0VLFT, etc.

Thank you,

Cristian

タグ(5)
0 件の賞賛
返信
1 解決策
1,889件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi Cristian,

Yes, as you can see in FACT SHEET S32K ISELED

https://www.nxp.com/docs/en/fact-sheet/S32K-ISELED-FS.pdf

For production, developers should order one of the S32K ISELED part numbers
below which include the full production license with unlimited driver functionality.

 

BR, Daniel

 

元の投稿で解決策を見る

1 返信
1,890件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi Cristian,

Yes, as you can see in FACT SHEET S32K ISELED

https://www.nxp.com/docs/en/fact-sheet/S32K-ISELED-FS.pdf

For production, developers should order one of the S32K ISELED part numbers
below which include the full production license with unlimited driver functionality.

 

BR, Daniel