I2C/SPI configuration and application example for S32K310

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I2C/SPI configuration and application example for S32K310

2,391 Views
Krishank
Contributor I

Hi, I am looking for S32K310 I2C and SPI application and configuration example. 

I am using S32DS IDE but all my examples are S32k1 based. 

Can someone attach example config/application for I2C and SPI peripheral for S32K310? 

0 Kudos
Reply
3 Replies

2,333 Views
Krishank
Contributor I

Thanks for you response. Can you send me the example for S32k311? or a link where I can refer the application code?

0 Kudos
Reply

2,316 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @Krishank 

You can download the S32K3 Real-Time Drivers Version 3.0.0 CD04 from S32K3 Standard Software > Automotive SW - S32K3/S32M27x - Real-Time Drivers for Cortex-M. 

VaneB_0-1722879067798.png

The .exe provides the plugins for EBTresos and also the sample codes and the updatesite.zip is for S32DS (S32DS Extensions & Updates: Explanation and How To Use and HOWTO: S32 Design Studio - Create a New S32DS Project from Example).

0 Kudos
Reply

2,363 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @Krishank 

As you know, S32K3 has many derivatives, so to reduce effort, in the most recent RTD releases we only provide examples for K344, K358, K288, and K396. Examples of other derivatives can be created based on these existing examples. 

The closest thing to what you are looking for would be the driver examples for S32K311 devices that are provided in the S32K3 Real-Time Drivers Version 3.0.0 CD04. Unfortunately, all software included in this release has Code Drop quality status in terms of testing is not fully tested. So, it is not recommended for production use but can be used as a reference.

 

BR, VaneB

0 Kudos
Reply