I cannot install S32K3xx Real-time Drivers AUTOSAR R21-11 Version 6.0.0 QLP01

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I cannot install S32K3xx Real-time Drivers AUTOSAR R21-11 Version 6.0.0 QLP01

ソリューションへジャンプ
2,262件の閲覧回数
marvincabuenas
Contributor II

Hi,

I recently have a S32K3X4EVB-T172 with a S32K244 microcontroller on it. I have followed all the instructions from Getting Started with the S32K3X4EVB-T172 Evaluation Board for Automotive General Purpose | NXP Semic... as well as Getting Started with the Real-Time Drivers (RTD) | NXP Semiconductors .

I installed the latest versions of what is currently available as of July 11, 2025. For some reason, I cannot install S32K3xx Real-time Drivers AUTOSAR R21-11 Version 6.0.0 QLP01.

Note: Screenshots are provided to show what software I have installed with my S32 Design Studio 3.6.2.

fail_to_install.pngfail_to_install.png

Screenshot 2025-07-11 095901.pngScreenshot 2025-07-11 095901.png

s32ds_sample_project list.pngs32ds_sample_project list.png

As a follow-up question just in case, if I'm able to install this, will I get the sample projects for the S32K344?

 

 

タグ(1)
0 件の賞賛
返信
1 解決策
2,252件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

The S32K3_S32M27x Real-Time Drivers Version 6.0.0 QLP01 is AUTOSAR R21-11 compliant. This release contains Crypto Driver.

Would you please install S32K3_S32M27x Real-Time Drivers ASR R21-11 Version 6.0.0 first? After installation you will get the S32K344 examples.


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
2,253件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

The S32K3_S32M27x Real-Time Drivers Version 6.0.0 QLP01 is AUTOSAR R21-11 compliant. This release contains Crypto Driver.

Would you please install S32K3_S32M27x Real-Time Drivers ASR R21-11 Version 6.0.0 first? After installation you will get the S32K344 examples.


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信
2,249件の閲覧回数
marvincabuenas
Contributor II

Hi Robin,

Thank you for the prompt reply. I'm now at the part of trying to debug the Port_Example_S32K344. The code can be compiled clearly but I'm having issues with the PEmicro Connection Assistant. Do you have further suggestions on what I can do?

Screenshot 2025-07-11 131540.pngScreenshot 2025-07-11 131540.png

I saw a previous thread saying something similar: Solved: An error occured while connecting to the interface hardware - NXP Community but I am unaware of any FAB pin.

0 件の賞賛
返信
2,240件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Please follow the steps shown in Getting Started guide: https://www.nxp.com/document/guide/getting-started-with-the-s32k3x4evb-t172-evaluation-board-for-aut...

By the way, did you Connect a micro-USB cable to the J40 connector to debug via the on-board S32K3 debugger?

0 件の賞賛
返信
2,235件の閲覧回数
marvincabuenas
Contributor II

Hi Robin,

I think my problem is the 12 volt adapter. Initially, I thought that just using the micro-usb for debugging would be enough to power on the board. Thanks again for replying quickly.

タグ(1)
0 件の賞賛
返信