s32k

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

s32k

1,426 Views
jayantxchauhan
Contributor I

HI NXP Community!

I'm trying to use the touch pad electrodes and the onboard potentiometer on the NXP S32k144EVB-Q100 with S32DS 3.4, Cannot find any example projects under RTM4.0, and have tried running these with BareMetal code, still couldn't figure out the errors, is there any SDK's that are compatible with S32DS 3.4 which consists any example project for these????

Kindly provide resources or another way to do this!!
@Robin_Shen @VaneB

0 Kudos
Reply
3 Replies

1,405 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Please contact NXP sales representatives for accessing materials. NDA required

By the way, I remember that these examples have not been updated for a long time, and they still use S32DS for ARM instead of the S32 Design Studio for S32 Platform 3.4 + SDK RTM 4.0.0 you mentioned.


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

1,395 Views
jayantxchauhan
Contributor I
Hi Robin, Can you confirm a thing, i have been informed that RTM 4.0 SDK is good for building applications for mass productions. is this correct, if so, what is the best IDE for using RTM 4.0 SDK. IS S32 Design Studio for S32 Platform 3.4 works best or are there any other versions. P.S : Using a S32k146 chip
0 Kudos
Reply

1,388 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Please note that SDK has been replaced by RTD, we always recommend the latest software such as S32K1 RTD 3.0.0.

0 Kudos
Reply