How to use DMA to get ADC result without interrupt in S32K344

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to use DMA to get ADC result without interrupt in S32K344

ソリューションへジャンプ
4,287件の閲覧回数
KerryJ
Contributor II

Hi, I want to learn How to use DMA to get ADC transformation result without ADC interrupt.

I used S32K344,

IDE is S32DS3.4 ,

RTD is S32K3 RTD AUTOSAR 4.4 VERSION 2.0.0

I am confused about how to config that.

Hope to get your help, thanks.

0 件の賞賛
返信
1 解決策
4,279件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信
8 返答(返信)
4,280件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信
4,254件の閲覧回数
KerryJ
Contributor II

thanks for your help, but my RTD VERSION IS 2.0.0. I can't run the project you give.

0 件の賞賛
返信
4,245件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

I added RTD200 version as well, so you can try.

BR, Petr

0 件の賞賛
返信
4,275件の閲覧回数
MVR
Contributor V

Hello @PetrS ,

In your example you used 5 ADC channels but in "Adc_Sar_Ip_1" you defined only 1 channel, is that correct?

MVR_0-1661463741717.png

Is it not necessary to put all channels in this array?

Thanks,

MVR

0 件の賞賛
返信
4,268件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

actually in this example BTCU is used to trigger conversions and command list is created with 5 commands.

PetrS_0-1661499829014.png

DMA then reads result from BCTU data register.

BR, Petr

0 件の賞賛
返信
4,235件の閲覧回数
MVR
Contributor V

Ok, I understand it,

But my question is: In "Adc_Sar_Ip_1" in the "Channel configurations array" option, don't you need to fill with the 5 channels used in your list?

0 件の賞賛
返信
4,225件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

the "Channel configurations array" option is for specifying which channels will be converted during normal conversion. It configs NCMRx registers. This is not used in the example

BR, Petr

4,218件の閲覧回数
MVR
Contributor V

Hmmm, I understand now! Thanks

0 件の賞賛
返信