How to program S32k144 with Multilink when use MBDT?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to program S32k144 with Multilink when use MBDT?

跳至解决方案
960 次查看
nujia
Contributor I

I use MBDT generate the code and program the S32k144 evb with OpenSDA interface.

but  i want to use Multilink to download the srec file. 

first step: generate the code wiht MBDT and compile the code.

second step: Run the S32DS, flash with elf file. 

How to automatic download the code without OpenSDA?

Thx.

0 项奖励
回复
1 解答
950 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi nujia,

The MBDT is currently supported on the MBDT community only.
The community is monitored daily by our experts on MBDT.
Can you please post the question there?
https://community.nxp.com/t5/NXP-Model-Based-Design-Tools/bd-p/mbdt
Thank you for your understanding!

You can refer to these two posts, but it is recommended to re-ask to get the latest answer:
Dears,how can i use multilink download code with Matlab Sumilink.
Flashing S32K144 with PEMicro Multilink from Toolbox

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
951 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi nujia,

The MBDT is currently supported on the MBDT community only.
The community is monitored daily by our experts on MBDT.
Can you please post the question there?
https://community.nxp.com/t5/NXP-Model-Based-Design-Tools/bd-p/mbdt
Thank you for your understanding!

You can refer to these two posts, but it is recommended to re-ask to get the latest answer:
Dears,how can i use multilink download code with Matlab Sumilink.
Flashing S32K144 with PEMicro Multilink from Toolbox

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复