S32K148 tested external flash ICs

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S32K148 tested external flash ICs

跳至解决方案
3,945 次查看
matej_15
Contributor III

Hi!

We are using FS32K148UJT0VMHR SMCU and we can't seem to find a list of tested serial flash ICs.

Usually, a supplier gives a list comprising of few ICs that have been tested. The only reference that is available is the devkit schematics which features MX25L6433FM2R-08G which is not automotive qualified.

Can you please point us or suggest an automotive qualified external serial flash ICs that is tested on QSPI or SPI interface of the S32K148 (64MB preferable)?

 

Best regards,

Matej

0 项奖励
回复
1 解答
3,896 次查看
davidtosenovjan
NXP TechSupport
NXP TechSupport

Yes, it should work.

在原帖中查看解决方案

5 回复数
3,928 次查看
davidtosenovjan
NXP TechSupport
NXP TechSupport

I have found in the internal resources, following two devices has been evaluated
- Macronix MX25l6433f (non AEC-Q100)
- Cypress S25FLxxxS

We don't have a list of validated QuadSPI flash ICs compatible with the S32K148, but the QSPI peripheral is generic and it should be compatible with most of the QSPI memories in the market.

There is an appnote providing general description of the QSPI module implementation in the S32K148, focused on setting up LUT sequences:
https://www.nxp.com/docs/en/application-note/AN12193.pdf

and accompanying software attachment:
https://www.nxp.com/webapp/Download?colCode=AN12193SW&docLang=en

3,924 次查看
matej_15
Contributor III

Hi @davidtosenovjan,

thank you for the answer!

If you could please also tell us can we use LPSPI in half-duplex parallel mode instead of QSPI interface? I see there is an option for LPSPI to have 4 data lines when in parallel mode:

matej_15_0-1655220234103.png

 

QSPI interfaces, both A and B, are unavailable in our application because of the use of RMII.

What is actually the difference between LPSPI in half-duplex parallel mode and QSPI? Performance, power consumption, etc?

 

Best regards,

Matej

0 项奖励
回复
3,909 次查看
davidtosenovjan
NXP TechSupport
NXP TechSupport

I have found an appnote dealing with LPSPI, it offers some power consumption saving features:

https://www.nxp.com/docs/en/application-note/AN5320.pdf

 

The biggest difference will be that QuadSPI offers memory mapped access - it means from application SW point of view you are accessing the same way as to internal RAM and you can even execute code directly over QuadSPI interface.

 

3,903 次查看
matej_15
Contributor III

Hi @davidtosenovjan,

 

so Cypress S25FLxxxS connected to S32K148 to LPSPI in half-duplex parallel mode should work, we just wouldn't be able to access it as the internal RAM?

0 项奖励
回复
3,897 次查看
davidtosenovjan
NXP TechSupport
NXP TechSupport

Yes, it should work.