How to program S32k144 with Multilink when use MBDT?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to program S32k144 with Multilink when use MBDT?

Jump to solution
959 Views
nujia
Contributor I

I use MBDT generate the code and program the S32k144 evb with OpenSDA interface.

but  i want to use Multilink to download the srec file. 

first step: generate the code wiht MBDT and compile the code.

second step: Run the S32DS, flash with elf file. 

How to automatic download the code without OpenSDA?

Thx.

0 Kudos
Reply
1 Solution
949 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi nujia,

The MBDT is currently supported on the MBDT community only.
The community is monitored daily by our experts on MBDT.
Can you please post the question there?
https://community.nxp.com/t5/NXP-Model-Based-Design-Tools/bd-p/mbdt
Thank you for your understanding!

You can refer to these two posts, but it is recommended to re-ask to get the latest answer:
Dears,how can i use multilink download code with Matlab Sumilink.
Flashing S32K144 with PEMicro Multilink from Toolbox

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
950 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi nujia,

The MBDT is currently supported on the MBDT community only.
The community is monitored daily by our experts on MBDT.
Can you please post the question there?
https://community.nxp.com/t5/NXP-Model-Based-Design-Tools/bd-p/mbdt
Thank you for your understanding!

You can refer to these two posts, but it is recommended to re-ask to get the latest answer:
Dears,how can i use multilink download code with Matlab Sumilink.
Flashing S32K144 with PEMicro Multilink from Toolbox

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply