How to config PDB in S32K144 using MCAL

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to config PDB in S32K144 using MCAL

跳至解决方案
1,653 次查看
wuxianlong
Contributor V

Hi,all

I can‘t find the way to config PDB to trigger ADC channel or group. Can you give me some information or suggestions, it is best to provide a hardware-triggered ADC demo.

* Autosar Version : 4.4.0
* Autosar Revision : ASR_REL_4_4_REV_0000
* Autosar Conf.Variant :
* SW Version : 1.0.1

BRs,
xianlong

0 项奖励
回复
1 解答
1,572 次查看
Nhi_Nguyen
NXP Employee
NXP Employee

Hi wuxianlong,

PDB used as default for S32K14X, so, you can find the example with trigger source is SW that was attached in the package with the link path: SW32K1_RTD_4.4_1.0.1\eclipse\plugins\Adc_TS_T40D2M10I1R0\examples.

For trigger source is HW, you can use one of them through this parameter:

Nhi_Nguyen_0-1694613408970.png

I attached the example for this. Please refer it.

 

Best regards,

Nhi

 

 

 

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,573 次查看
Nhi_Nguyen
NXP Employee
NXP Employee

Hi wuxianlong,

PDB used as default for S32K14X, so, you can find the example with trigger source is SW that was attached in the package with the link path: SW32K1_RTD_4.4_1.0.1\eclipse\plugins\Adc_TS_T40D2M10I1R0\examples.

For trigger source is HW, you can use one of them through this parameter:

Nhi_Nguyen_0-1694613408970.png

I attached the example for this. Please refer it.

 

Best regards,

Nhi

 

 

 

0 项奖励
回复