How to config PDB in S32K144 using MCAL

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to config PDB in S32K144 using MCAL

ソリューションへジャンプ
1,778件の閲覧回数
wuxianlong
Contributor V

Hi,all

I can‘t find the way to config PDB to trigger ADC channel or group. Can you give me some information or suggestions, it is best to provide a hardware-triggered ADC demo.

* Autosar Version : 4.4.0
* Autosar Revision : ASR_REL_4_4_REV_0000
* Autosar Conf.Variant :
* SW Version : 1.0.1

BRs,
xianlong

0 件の賞賛
返信
1 解決策
1,697件の閲覧回数
Nhi_Nguyen
NXP Employee
NXP Employee

Hi wuxianlong,

PDB used as default for S32K14X, so, you can find the example with trigger source is SW that was attached in the package with the link path: SW32K1_RTD_4.4_1.0.1\eclipse\plugins\Adc_TS_T40D2M10I1R0\examples.

For trigger source is HW, you can use one of them through this parameter:

Nhi_Nguyen_0-1694613408970.png

I attached the example for this. Please refer it.

 

Best regards,

Nhi

 

 

 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,698件の閲覧回数
Nhi_Nguyen
NXP Employee
NXP Employee

Hi wuxianlong,

PDB used as default for S32K14X, so, you can find the example with trigger source is SW that was attached in the package with the link path: SW32K1_RTD_4.4_1.0.1\eclipse\plugins\Adc_TS_T40D2M10I1R0\examples.

For trigger source is HW, you can use one of them through this parameter:

Nhi_Nguyen_0-1694613408970.png

I attached the example for this. Please refer it.

 

Best regards,

Nhi

 

 

 

0 件の賞賛
返信