How to add port config in CAN demo of RTD 6.0.0 in S32DS 3.6.3

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to add port config in CAN demo of RTD 6.0.0 in S32DS 3.6.3

Jump to solution
165 Views
chenwilsoft
Contributor II

The version of S32DS for S32 platform is 3.6.3. The version of RTD for S32K3 installed is 6.0.0.

I select Create Application from Example and select Can_Example_S32K344. I want to add the MCAL Port. After the port added, there are errors showed. "There must be at least one configuration" and "Name must be a valid C identifier". But I could not find the place to fix the errors.

chenwilsoft_0-1755509341242.png

 

 

 

 

0 Kudos
Reply
1 Solution
148 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

you should add desired pins in Pins Tool. Also name functional group properly

PetrS_0-1755514419406.png

PetrS_1-1755514426970.png

BTW: you can refer to below demos
https://community.nxp.com/t5/S32K-Knowledge-Base/RTD600-MCAL-amp-IP-S32K3X4EVB-T172-FlexCAN-Example-...

BR, Petr

 

View solution in original post

0 Kudos
Reply
1 Reply
149 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

you should add desired pins in Pins Tool. Also name functional group properly

PetrS_0-1755514419406.png

PetrS_1-1755514426970.png

BTW: you can refer to below demos
https://community.nxp.com/t5/S32K-Knowledge-Base/RTD600-MCAL-amp-IP-S32K3X4EVB-T172-FlexCAN-Example-...

BR, Petr

 

0 Kudos
Reply