How to add port config in CAN demo of RTD 6.0.0 in S32DS 3.6.3

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to add port config in CAN demo of RTD 6.0.0 in S32DS 3.6.3

跳至解决方案
166 次查看
chenwilsoft
Contributor II

The version of S32DS for S32 platform is 3.6.3. The version of RTD for S32K3 installed is 6.0.0.

I select Create Application from Example and select Can_Example_S32K344. I want to add the MCAL Port. After the port added, there are errors showed. "There must be at least one configuration" and "Name must be a valid C identifier". But I could not find the place to fix the errors.

chenwilsoft_0-1755509341242.png

 

 

 

 

0 项奖励
回复
1 解答
149 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

you should add desired pins in Pins Tool. Also name functional group properly

PetrS_0-1755514419406.png

PetrS_1-1755514426970.png

BTW: you can refer to below demos
https://community.nxp.com/t5/S32K-Knowledge-Base/RTD600-MCAL-amp-IP-S32K3X4EVB-T172-FlexCAN-Example-...

BR, Petr

 

在原帖中查看解决方案

0 项奖励
回复
1 回复
150 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

you should add desired pins in Pins Tool. Also name functional group properly

PetrS_0-1755514419406.png

PetrS_1-1755514426970.png

BTW: you can refer to below demos
https://community.nxp.com/t5/S32K-Knowledge-Base/RTD600-MCAL-amp-IP-S32K3X4EVB-T172-FlexCAN-Example-...

BR, Petr

 

0 项奖励
回复