How is the Doze mode working in S32K series

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How is the Doze mode working in S32K series

ソリューションへジャンプ
2,565件の閲覧回数
176211901
Contributor I

how dose the Doze mode working in S32K series peripheral?

I see the Doze mode in S32K reference manual, but I didn't see the details that how it is working.

タグ(1)
0 件の賞賛
返信
1 解決策
2,417件の閲覧回数
jorge_a_vazquez
NXP Employee
NXP Employee

Hi wang jian

DOZE mode can optionally keeps peripheral on or off, in Low Power modes. In this way, for example, communication peripheral (LPSPI, LPUART, etc) allow the application to receive data while core is in low power mode.

For your reference please check this link:

Low power and Doze Mode question in S32K 

 


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
-------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,418件の閲覧回数
jorge_a_vazquez
NXP Employee
NXP Employee

Hi wang jian

DOZE mode can optionally keeps peripheral on or off, in Low Power modes. In this way, for example, communication peripheral (LPSPI, LPUART, etc) allow the application to receive data while core is in low power mode.

For your reference please check this link:

Low power and Doze Mode question in S32K 

 


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
-------------------------------------------------------------------------------

0 件の賞賛
返信
2,417件の閲覧回数
176211901
Contributor I

Thanks for your reply.

There is a another question:

what is the difference between DOZEN and MEN in LPSPI Control Register ?

 

0 件の賞賛
返信