How about S32K SPI bitsPerSec when work at master mode?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How about S32K SPI bitsPerSec when work at master mode?

2,024件の閲覧回数
hansonhe
NXP Employee
NXP Employee

Dear,

We set S32K lpspiSrcClk=56000000U, how about the SPI bitsPerSec when work at master mode?

now we could only achieve 7000000U, Thanks. We want to achieve 28000000U.

0 件の賞賛
返信
2 返答(返信)

1,776件の閲覧回数
razva_tilimpea
NXP Employee
NXP Employee

Hi,

If you want to use the LPSPI at high clock speed is mandatory to use it in DMA mode.

I will try to come back with a working project, but I think that your clock speed it too high.

Best regards,

Razvan

0 件の賞賛
返信

1,776件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

The max SPI baud rate is 24MHz in high speed mode as per the datasheet.

BR, Petr

0 件の賞賛
返信