How about S32K SPI bitsPerSec when work at master mode?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How about S32K SPI bitsPerSec when work at master mode?

2,090 Views
hansonhe
NXP Employee
NXP Employee

Dear,

We set S32K lpspiSrcClk=56000000U, how about the SPI bitsPerSec when work at master mode?

now we could only achieve 7000000U, Thanks. We want to achieve 28000000U.

0 Kudos
Reply
2 Replies

1,842 Views
razva_tilimpea
NXP Employee
NXP Employee

Hi,

If you want to use the LPSPI at high clock speed is mandatory to use it in DMA mode.

I will try to come back with a working project, but I think that your clock speed it too high.

Best regards,

Razvan

0 Kudos
Reply

1,842 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

The max SPI baud rate is 24MHz in high speed mode as per the datasheet.

BR, Petr

0 Kudos
Reply