I can't read the data from 24c02.
Hi,
What do you see on scope? It is trying to write to the 24c02?
You have to use pull-up. Internal pull-ups are disable in this example.
You can enable them in PORTA[PCR] registers.
Regards,
Daniel
Dear:
Can you help me test it?
Hi,
The configuration is correct.
Only generate Processor expert code, it should work.
Regards,
Daniel
Hi,
Can you be more specific? What exactly you need to know?
If you need to use pins 6/7 instead of pins 0/1 which are selected in this example by default, you must change routing of the pins in the pin_mux driver as well.
Regards,
Daniel