FreeRTOS_Toggle_Led_Example_S32K344 stuck in prvPortStartFirstTask

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FreeRTOS_Toggle_Led_Example_S32K344 stuck in prvPortStartFirstTask

1,837 Views
lucianmocanu_zzzzz
Contributor II

Hello,

Same issue as here:https://community.nxp.com/t5/S32K/FreeRTOS-stuck-in-prvPortStartFirstTask/td-p/1418594

I already have the versions packages required for FreeRTOS and RTD:

SW32K3_RTD_4.4_2.0.1_DS_updatesite_D2207

SW32K3xx.S32DS_3.5.0_D2212

SW32K3_FreeRTOS_10_4_6_UOS_2_0_1_DS_updatesite_D2209

 

In the original post it doesn't say what the root cause is and how it is later "fixed".

Can we get some information on how to fix this?

 

Thank you,

Lucian

 

0 Kudos
Reply
4 Replies

1,441 Views
SandyHCL
Contributor I

FreeRTOS_Toggle_Led_Example_S32K312. Can anyone tell me what are supporting packages need to be downloaded for making this example code build?

0 Kudos
Reply

1,778 Views
lucianmocanu_zzzzz
Contributor II

Hi Dan,

It does work without the J-Link however I don't have a different debugger.

Do you know of any workaround to be able to use the J-Link?

Thank you,

Lucian

0 Kudos
Reply

1,776 Views
DanNguyenDuy
NXP Employee
NXP Employee

Hi lucianmocanu_zzzzz,

Unfortunately, I don't know of any workaround to be able to use the J-Link.

Best regards,

Dan

0 Kudos
Reply

1,792 Views
DanNguyenDuy
NXP Employee
NXP Employee

Hi lucianmocanu_zzzzz,

The first: Based on your attached link, in my opinion, this issue occurred when they used SEGEGR J-Link debugger. Could you try to use the PNE or Launter bach debugger to re-test?

The second, in the Release Note of FreeRTOS version 2.0.1 was noted:

Make sure S32 Design Studio v3.4, S32 Design Studio for S32 Platform v.3.4 Update 3 EAR 
with S32K3 Service Pack (SW32K3_S32DS_3.4.3_D2112.zip) and S32K3 RTD 2.0.1 package 
are installed before this FreeRTOS package.

Could you re-check installing from your side? 

Best regards,

Dan

0 Kudos
Reply