Flash Programming in S32DS for S32 Platform

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Flash Programming in S32DS for S32 Platform

Jump to solution
6,313 Views
gpira
Contributor III

Hi everyone,

I'm currently working with S32 Design Studio for S32 Platform v. 3.4 and it occurs to me that there isn't direct flash programming option.

Is the debug feature the only way to program my micro (I'm using a S32K144)?

Also, how could I perform a memory dump of my program? 

I used the Flash Programmer Task in Code Warrior when I was working with a 9S12ZVC and it worked perfectly, is there something similar for the S32K1?

Thanks.

Best regards,

Giacomo

0 Kudos
Reply
1 Solution
6,305 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@gpira

you can take a look at the documents :

PnE_GDB_Server_Debug_Configuration_User_Guide.pdf

this documents under you install path,such of mine:C:\NXP\S32DS.3.4\S32DS\help\pdf

Senlent_0-1649387580356.png

I don't know if this infos you are looking for.

BR!

      Jim,

 

View solution in original post

0 Kudos
Reply
5 Replies
6,306 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@gpira

you can take a look at the documents :

PnE_GDB_Server_Debug_Configuration_User_Guide.pdf

this documents under you install path,such of mine:C:\NXP\S32DS.3.4\S32DS\help\pdf

Senlent_0-1649387580356.png

I don't know if this infos you are looking for.

BR!

      Jim,

 

0 Kudos
Reply
6,297 Views
gpira
Contributor III

There were quite useful, but it seems that what I was looking for isn't yet implemented for 

the S32 Platform version of S32DS. 

For example, in this post HOWTO: download separate elf/srec/hex file to microcontroller using S32 Design Studio  your colleague refers to the flash programming support in IDE (the one with the Lightning symbol), but for what I've understood this feature is only available in S32DS PA, am I right?

Do you plan on adding this functionalities also in S32DS for S32 Platform? 

Thanks,

Giacomo

0 Kudos
Reply
6,290 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@gpira

I don't see any difference, I feel that the function is the same, but there is no shortcut icon

0 Kudos
Reply
6,288 Views
gpira
Contributor III

The difference is in terms of time, because everytime it starts the debug procedure, while I simply wanted to load my code into the flash

0 Kudos
Reply
6,284 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@gpira

I guess no such update in the future.

BR!

     Jim,