"arm-none-eabi-gcc" and "arm-none-eabi-g++" not found in PATH

cancel
Showing results for 
Search instead for 
Did you mean: 

"arm-none-eabi-gcc" and "arm-none-eabi-g++" not found in PATH

Jump to solution
680 Views
Raphael2
Contributor III

Hi,

I work with the S32k144 and design studio 2018.R1.

I tried to import and debug a project, but:

Raphael2_0-1626682096649.png

these errors appear after importing the project and:

Raphael2_1-1626682164245.png

these join them after I build 'Debug_Flash'.

In another post installing 'gcc-arm-none-eabi-10-2020-q4-major-win32.exe' was the solution, but I just installed it and there is no change.

Hope someone knows what this means.

 

Best regards,

Raphael

0 Kudos
1 Solution
664 Views
Raphael2
Contributor III

Installing S32 Design Studio 3.4 and adding Service pack 1 solved my problem

View solution in original post

0 Kudos
2 Replies
163 Views
勝民
NXP Employee
NXP Employee

One solution would be to set the PATH variable to a toolchain of choice, either per project or to the entire editor, as shown below:

_0-1649420598238.png

 

0 Kudos
665 Views
Raphael2
Contributor III

Installing S32 Design Studio 3.4 and adding Service pack 1 solved my problem

0 Kudos